This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL536A CB引脚电压

Other Parts Discussed in Thread: BQ76PL536A

请教用过这款芯片的朋友,BQ76PL536A 的 CB_CTRL 寄存器对应位设置为 1 时——即开始均衡, CB(n) 引脚与VC(n-1)引脚之间的电压差是多少呢?

数据手册上(附件)也没写具体能输出几伏电压。

我测到的电压为1.6V左右,这个电压开通不了MOS管,难道还得外加驱动电路?

谢谢!

  • 不均衡时CBn应该接近VCn-1,在做均衡时CBn应该接近VCn。

    可能需要检查一下VCn和VCn-1之间的电压是否正常。

  • 非常感谢!

    已经测试出,在不驱动MOS时,电压可以在您所说的范围内变化,接上MOS管之后就会出现这个问题。

    之前也是参照数据手册上的典型应用电路图,上面均衡的MOS用的是FDN359AN,封装是SOT23,查看MOS管手册发现这个MOS 3V电压就能驱动,因为我的均衡功率要比官方的Demo板大的多,所以选了一个封装是TO-252AA的 MOS,这个MOS 3V也可以驱动开通,但现在测下来 BQ76PL536A 的驱动能力有限,驱动不了,还要外加驱动电路。

  • 还得再麻烦您一下,我现在用4片级联,每片采集5节电池的信息,原理图是参考 EVM-3,layout 布线与 EVM-3几乎一样,现在的问题是只能寻址到第一片芯片,第二片都寻址不到,第一片芯片可以准确的读回电池信息。

    我的板子只用了SPI几个端口,FAULT_H、ALERT_H、DRDY_H、CONV_H几个引脚没有使用, 也是从论坛上了解,CONV_H如果不用要接低,已经拉低了。

    我有一点不理解的是:我用示波器测量测,第一片因为参考地就是系统的GND,所以SPI几根数据线的电平都是正的;而第二片的参考地是第一片的供电电压,同样我用示波器测试的时候,CS_S、SDI_S、SCLK_S电平信号全是负的,SDO_S没有信号,这波形正常吗?

    谢谢!