This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8864-Q1: 咨询BOOST 升压恒流芯片

Part Number: LP8864-Q1

当前有一个需求,就是16个灯串,电压是45V到60V之间,每一路最大电流100MA

希望能够实现1:3000的PWM调光深度。

此外,每个灯串希望能够共阳极,但是负端需要单独控制。

因此,请告知TI是否有合适的芯片选择,目前找到的都是4通道的芯片,这样会导致有限的板子空间上要放4个芯片。希望能找到最少8通道或者16通道的芯片,能满足此要求的芯片。