Part Number: LM5012
- LM5012 48V输入,24V输出,无论负载电流多大,输出纹波都有400mV以上
- 原理图

- PCB 图纸


- 输出纹波如下分别为1.6A负载和0.6A负载时纹波


- 测量方式如下图

- 期待您的回复!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
在芯片数据手册中推荐使用铁氧体芯的电感。
LM5013-Q1EVM 评估板 | 德州仪器 TI.com.cn 评估板使用的电感是74437368220,这是电感的数据手册
ttps://www.we-online.com/components/products/datasheet/74437368220.pdf
对比74437368220手册,PSPMAA1265H-680M-ANF手册显示是1265 Series 68uh,其电气指标是基于100KHZ/1V测试的,Saturation Current@30%只有5.5A。
“9.2.2.7 Type 3 Ripple Networ” 是为了提供更低的纹波,但现在的纹波(400mV) 指标,我认为和L1 R11 C9的选值关系不大,和选型更相关。
当然,这个SNVR514 Calculation tool | TI.com工具可帮助如何获得更低的纹波。