This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: Dual rail synchronous rectification

Part Number: UCC28950

Hello

Hope you are having a good day

 I am planning to do 3KW PFC+FULL Bridge switch mode power supply. UCC28950ic is the heart of it.

the desired output is +-170Vdc and i want to use SR to increase efficiency at the secondary side.

with the help of your WEBENCH tool i got a rough  idea only for a single rail output variant.

Could you give me an advice on how dual rail output could be implemented with E and F output of the UCC28950, if possible  of course.

Thank you in advance

Best Regards,

Saba