This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54231,影响最大输出电流的关键点

Other Parts Discussed in Thread: TPS54231

24V转5V的电路,使用TPS54231,驱动点阵显示,行扫描。发现一个问题,如果此行需要显示的点数多时,相对于显示点数少的行,亮度会有所下降。考虑可能与电源最大输出电流有关。因此想咨询,哪些关键点涉及TPS54231最大输出电流?

  • 你的意思是用多个54231,每个给一行点阵驱动?显示点数多的亮度差一些?那你点数多的输出电压是否有变化?可能跟电感关系大一些。

  • TPS54231是2A输出降压型DC/DC芯片,最大输出电流主要受限与内部的OCP电流保护,规格是2.3~5.3A,  按照电感的峰值电流IL= Ioutmax+ ILripple/2 , 所以最大输出电流实际和电感的纹波电流ILripple有关,而ILripple电流取决于输入输出电压,电感感量,频率。(见datashee:www.ti.com.cn/.../tps54231.pdf 第十三页公式8,KIND*Iout实际就是ILripple.

    另外见datasheet 第六页Figure 8, OCP电流保护会受到芯片结温,输入电压影响。

  • 好的,谢谢 wei wang 和 Johnsin Tao。

    又通过其他方法测试了一下,不同行显示亮度有差异不是电源这部分的问题,可能是点阵显示的常见现象。

    谢谢。