BQ34Z100在放电过程中发生跳变,15A,7.2V磷酸铁锂电池,静置后电池电压7.07V,RemCap 和FullChgCap都是14540MA,开始用1.5A放电,电压很快降到6.4V左右,剩余电量在14395的时候一下子跳到了4366,SOC因此由100%变成了31%,感觉一下子少了10000MA,这个是怎么回事呢?麻烦帮我看一下,谢谢! ‘
附件里面是GG文件和LOG文件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ34Z100在放电过程中发生跳变,15A,7.2V磷酸铁锂电池,静置后电池电压7.07V,RemCap 和FullChgCap都是14540MA,开始用1.5A放电,电压很快降到6.4V左右,剩余电量在14395的时候一下子跳到了4366,SOC因此由100%变成了31%,感觉一下子少了10000MA,这个是怎么回事呢?麻烦帮我看一下,谢谢! ‘
附件里面是GG文件和LOG文件
从你的GG文件看,Update Status=04,阻抗也没有更新,Qmax也没更新。这说明还没有做golden learning。所以这个时候说SOC精度是没有意义的。
建议先做完golden learning,看到Update Status=06,阻抗和Qmax也更新了,再做相同的测试看看结果如何。