This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27541低温电量跳变问题



    电池放在温度箱里面(没有充放电),设定温箱温度从常温降到-20度,运行后,当温度降到到-6度左右电量从52%跳变为0,温度降到-20度以后,开始升温,当温度升高到4度左右电量又从0跳变到51%;什么原因?如何解决?

  • 这是正常的,电池本身在低温下显著增加内阻,导致电池可用能量急剧减少。

    可以在Pack Configuration [RCJUMPOK] 改为0 ,可以防止跳变。但是要注意,一旦在低温下放电,依然有可能会跳变到0