如上图所示,采用两个电池给主板(PCB)供电,充电电路也在主板上,因此主板的地GND应该就是充电电路和负载电路的负极应该接在手册电路的PACK-上,电池的正负极分别接TB3的1,2脚,因此充电电路的地对应的就应该是两个电池的负极即为GND1-和GND2-
现在的问题是在实际使用中打算用P3和P4的IIC接口通过EV2300给芯片配置学习好了的参数,然后在使用中通过主板上的单片机IIC来读取电量,那么BQ34Z100电路的IIC接口上的地怎么接呢,他们的地是GND1-和GND2-,可是单片机的地是GND,不共地了,这几个地应该怎么处理呢?还是说这个IIC接口不能让EV2300和单片机公用?