This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2776提供负电压输出不对

Other Parts Discussed in Thread: LM2776

最近使用LM2776提供负电压,输入+5V,希望得到-5V的电压输出。电路如下(根据数据手册第一页图绘制):

现在的问题是:

给ASM1117-5.0提供+7V电压,电源显示电流0.005A = 5mA;然后由得到的约+5V电压(实测为+4.945V)作为LM2776的输入,跨接电容(图中C42)为瓷片电容1uF,输出-1.554V。在LM2776的输出端并联接了一些钽电解电容,应该属于空载。

当跨接电容为极性电容时(1uF钽电解电容),输出-1.999V。

请帮忙解释这是什么原因?如何解决?