This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: BQ25756 无法获取光伏板电流。在光伏电压低于4.2V时。

Part Number: BQ25756

1.使用BQ25756设计光伏充电器时,需要获取光伏短路时的电流。目前遇到的问题,通过外部MOS管将输入测流电阻对地短路,无法获取短路时的电流,但是短路时电压可以获取。

2.使用光伏模拟器,作为输入设置VOC=4.2V,ISC=0.5A,可以读取短路时电流。VOC=4.1V,ISC=0.5A,条件下就无法获取短路电流。

3.输入电流读取有什么前提条件吗,如何才能在短路的情况下也能读取电流值。