之前用到了颗TPS7A6650-Q1芯片,用于输出5V给外围传感器供电,在测试中短GND测试正常,短12V时烧毁。
1、有没有能防止短地和短电源的5V LDO产品?
2、如果外部加一个防反二极管可以避免短电源问题,但是输出电压由于二极管压降又比5V低了。有没有更好的方案?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前用到了颗TPS7A6650-Q1芯片,用于输出5V给外围传感器供电,在测试中短GND测试正常,短12V时烧毁。
1、有没有能防止短地和短电源的5V LDO产品?
2、如果外部加一个防反二极管可以避免短电源问题,但是输出电压由于二极管压降又比5V低了。有没有更好的方案?
你好,
我好像回复了这个帖子,可以使用TPS7B4253-Q1来解决问题,关键在输出端是40V的耐压,这样短到电池也不会坏。