使用bq34z100 EVM。完成learned cycle 后updata status跳06
1.是否代表学习完成?
2.学习完成后是否需要下其他命令去锁定内部Data memory设定值?
若我电池继续充放电后会不会再更改到Data memory设定值?
3.QEN是否一按下IT enable后变成红灯,学习完成之后不会再变成绿灯?这样是否正确?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用bq34z100 EVM。完成learned cycle 后updata status跳06
1.是否代表学习完成?
2.学习完成后是否需要下其他命令去锁定内部Data memory设定值?
若我电池继续充放电后会不会再更改到Data memory设定值?
3.QEN是否一按下IT enable后变成红灯,学习完成之后不会再变成绿灯?这样是否正确?
1,还需要看一下Qmax,Ra Table更新是否正常。
2,可以发0x0020命令进行上锁。
3,QEN学习后不会变成绿灯。
1.Qmax与Ra Table更新如何算正常?是否可以透过观看MaxError() Updates =1%表示正常
2.进行量产時是否将golden汇出的.srec档案programming在新ic上然后再发 0x0020命令进行上锁