Part Number: BQ76942
能不能问一下,我的MCU是通过BQ76942的REG1供电的,当我MCU发送RESET命令给bq76942后,MCU好像也发生了复位,我想问一下发送RESET命令后是不是REG1会短暂掉电,然后重新上电导致MCU发生复位。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ76942
能不能问一下,我的MCU是通过BQ76942的REG1供电的,当我MCU发送RESET命令给bq76942后,MCU好像也发生了复位,我想问一下发送RESET命令后是不是REG1会短暂掉电,然后重新上电导致MCU发生复位。
你是否注意到在复位命令期间REG1 LDO电压降为0V?你是否使用了0x0012 RESET()命令?
我用示波器抓过了,并没有抓到LDO下降的情况,我使用了0x0012reset命令
不建议使用PF_RESET命令,因为它可能会禁用某些功能。这是一种永久性故障复位,这意味着设备达到了永久性故障,导致IC禁用。PF_RESET命令应重置设备,但它会禁用某些操作所需的功能。
我又抓了一遍发现reg1会有一瞬间的跌落的现象3.3V降到2.2V
添加适量的额外电容是否会使电压保持在足够高的水平,以阻止MCU重置.