This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP3907: When reading the registers of the LP3907SQ-JXQX/NOPB via I2C, there is an ACK, but the data of all registers are 0xFF.

Part Number: LP3907

When I was configuring the output of LP3907SQ-JXQX/NOPB using I2C, I found that the values of all the registers of this chip were all 0xff. However, when I used a logic analyzer to capture the data, I found an ACK signal. Additionally, testing the other two devices on this I2C bus showed that they could read and write normally. Could it be that I have overlooked some necessary read/write operations for this chip?The figure below shows the data captured by the logic analyzer.

Snipaste_2026-03-19_20-33-58.png