我的系统是单节锂电池供电的,需要usb或AC适配器充电。电池供电给一个GSM模块(4V左右,发送瞬间电流2A),其他电源需要5V/100mA,3.3V/100mA,可选5V或3.3V200mA 。产品需要低功耗设计,使用430主控。我找不到合适的电源芯片。GSM现在处理是电池直连,感觉不是很好的方式。请专家指点
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
充电部分可以选择带电源电源路径管理的电池充电芯片:bq24160 ,BQ24052,等
BQ24052: www.ti.com.cn/.../bq24052.pdf
BQ24161: www.ti.com.cn/.../bq24161.pdf
更多选择:focus.ti.com.cn/.../parametricsearch.tsp
AC适配器芯片可以选择UCC28610:见参考方案: www.ti.com.cn/.../pmp4305 (可修改整流方式)
锂电池4.2V转4V选用:TPS63020/1: www.ti.com.cn/.../tps63020.pdf 等
锂电池4.2V转5V选用:TPS61093: www.ti.com.cn/.../tps61093.pdf 等
锂电池4.2V转3.3V选用:TPS63030 : www.ti.com.cn/.../tps63020.pdf 等
kai fang,
想请教下:这个系统对电源供电方案的整体大小有没有要求?锂电池的供电截止电压是多少?GSM是电池直连,那其他3.3V@200mA是使用什么芯片?以下推荐一种方案, 供参考。
采用两个DC/DC供电:GSM 4V@2A可以采用BUCK-BOOST的TPS63020, 相比于电池直接供电,其负载调整率高;另外3.3V@200mA可以采用TPS62240。