Part Number: TPS7A8300
1.给该芯片输入3.9V,输出3.45V。
2.当负载电流由10mA上升到550mA后,输出电压下降了300mV。
3.输出电压下降大,与规格书数据测试的不一致,请问如何解决,以及原因是什么。谢谢!
1.Applying 3.9V to the input of the chip,and output voltage is 3.45V.
2.When the load current increases from 10mA to 550mA, the output voltage drops by 300mV.
3.The voltage drop is too big,and how can I resolve this? Thanks!