Other Parts Discussed in Thread: TPS40060, LM5116, LM5117
请问:我要设计一款降压型DC/DC,输入26V到32V,输出24V/3A。初步比较了LM5116/7、TPS40060/1,感觉都可以,不知该选用哪一款控制芯片最优?希望效率最高、体积最小。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi 可以用TI的webench输入规格,里面会列出TI符合规格的芯片,里面有size和效率等各种指标的比较
http://www.ti.com/lsds/ti/analog/webench/overview.page
你好
LM5117可以的。可以去WEBENCH做设计和仿真,以下是相关介绍资料:
http://www.deyisupport.com/question_answer/analog/power_management/f/24/t/106522.aspx
还有其它的要求么?比如保护,纹波,调整率,发个详细的要求,webench可以提供很好的支持。
你好,LM5116和LM5117的差别仅在于输入电压范围不同,其余管脚兼容吗?
谢谢关注!
我想做一款输入26V到36V,输出10V到24V可调,输出电流最大5A的BUCK,要求电压调整率和负载调整率不大于2%,纹波小于100mv,具有过流(140%)保护功能。希望体积小,效率高(大于90%)。
你是专家,请给建议。再次感谢!!