This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: The wafer diameter used in the official mass production batches of BQ40Z50

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQ40Z50

Dear TI Technical Support Team,
 
Our company is currently using the BQ40Z50 chip in mass production projects. For the needs of product reliability verification, supply chain cost analysis and production process matching, we sincerely ask for your assistance to provide the core process parameters of this chip, the specific requirements are as follows:
 
1. The wafer diameter used in the official mass production batches of BQ40Z50 (please specify whether it is 200mm/8 inches or 300mm/12 inches);

2. The process node and process type corresponding to this chip (such as specific information like 130nm BCD high-voltage process);

3. The die size of the chip (including length × width specification and die area).
 
Please provide official and accurate data. If some internal confidential information is involved, non-public reference values applicable to the project can be provided. Thank you for your support and assistance!

  • Hello, we have received your case and the investigation will take some time. Thank you for your patience.

  • The TI forum aims to address technical issues customers encounter while using TI products. We recommend contacting the customer support department via the following methods, where representatives will assist you.
    • Open the link ticsc.service-now.com/csm
    • Click the "Submit Application" button under "Apply for New Support"
    • Click the "Create Case" button under "Other" in the newly opened window
    In the opened table, you can describe your issue in Chinese and submit it.