Part Number: LM5156
1、LM5156芯片,在BIAS外部输入大于3.6V电压时,最小升压电压=1.5V(Vin)。没有说明这个外部3.6V电源的电流应该多少A。另外,运用电路设计器WEBENCH,最小输入电压填写是几伏。1.5V它也不认啊。请给我指点一下,所有可以用BIAS输入辅助电源的芯片都可以用你解答的方法来计算电路?
2、电路在BIAS电压的输入,实现了低电压启动。启动以后,可否用输出电压来供电(假定输出电压大于3.6V)。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
– Minimum boost supply voltage 1.5 V whenBIAS ≥ 3.5 V
为了实现电路的输入电压最小为1.5V,我用一个5V的外接电源到BIAS引脚。这个5V的外接电源的负载能力是0.2A,也就是说外加在BIAS引脚上的电源是5V0.2A。问:这个电源(5V0.2A)能否使得LM5156在输入电压1.5-2.4V时,正常工作?我担心BIAS输入的5V0.2A的驱动能力太小,所以,问你BIAS引脚上加多大的驱动电流合适。
我现在应用场景是:输入电压:1.5-2.4V时;BIAS电压:5V0.2A,输出电压:6V2A,如何应用电路设计器WEBENCH?在你的电路目录中有不少芯片是带BIAS管脚的。我想了解一下你的解决方法。
第2个问题就不纠缠了。电路能够正常工作了,我再慢慢地试验。
按照WEBENCH® Designer LM5156的输入范围,应该是无法使用WEBENCH进行设计。
您可以试下 LM5155x / LM5156x Boost Quick Start Calculator这个计算表格: