你好,我想将DC/DC输出的5V/500mA的纹波电压降下来,打算通过TPS61220升压到6V,再用TPS7A4700降至5V,不知可行不?最后输出的5V能有多大电流输出?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
tps61220的输出电路达不到500mA,请问输入电压范围是多少?
LDO建议选用TPS7A8101,这个电压范围更合适。
你好,是这样,我有一个采集板,供电是另一个板子电源板的DC/DC通过引线过来的5V(最大电流 500mA)。我的需求是将这个DC/DC过来的5V纹波降下来以供采集板使用。方案是通过tps61220升压至6V后再用LDO TPS7A4700将电压再降至5V。请问升压到6V,能有多大的电流输出呢?再者,板子空间有限,选用TPS7A4700恰好可以通过调整LAYOUT输出,无需太多外围器件,节省空间。只是不知道最后TPS7A4700输出5V时能输出多大电流?不只这样考虑可行否?谢谢。
Hi
TPS61220的开关电流只要240mA, 要想输出500mA必须选择MOS最低限流在700mA以上的芯片。
或可以选择TPS61252: http://www.ti.com/lit/ds/symlink/tps61252.pdf