This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: LM5022的电流检测和电流限制功能CS引脚可以直接接GND吗?

Part Number: LM5022

各位工程师好!有个问题向各位请教:我在用LM5022准备搭一个sepic升降压电源电路,针对负载峰值功率的降额设计足够大,设计输出功率是实际负载峰值功率的3倍多,大部分时间又都是轻载小电流状态,所以不想用CS引脚的电流检测和过流保护功能了,可以把电流采样电阻RSNS去除后CS引脚直接接GND吗?相应的LM5022 Datasheet典型应用电路图中连到CS pin脚的低通滤波RS1、Ccs及Rs2可以全部去除吗?请指导,谢谢!

  • 您好,

    感谢你提出问题,并考虑在设计中考虑LM5022。

    即使不需要电流限制功能,LM5022 仍应保留电流感应电阻。主要原因是LM5022的控制环路是峰值电流模式控制。移除电流感应电阻会改变控制环路,设计可能不稳定。

  • 好的,谢谢!那我照常保留,按0.5V/sepic耦合电感峰值电流的阻值,再偏小一点设置RSNS,谢谢您。

  • 你好,继续请教下问题,我搭这个sepic电路是给BLDC电机母线供电,峰值功率18W左右,通过MCU输出可调占空比的PWM经过RC低通滤波和电压跟随器到LM5022的VFB引脚调节sepic输出电压,那我LM5022外围的PCB该如何布局布线?看到"AN-1557 LM5022 Evaluation Board"https://www.ti.com/lit/ug/snva203c/snva203c.pdf中两层评估板是把欠压保护UVLO的下拉电阻RUV1、软启动Css电容、频率电阻RT的信号GND端单独铺一小块铜皮,然后单独单点接地到输入输出功率地GND的大铜皮上。

    既然LM5022是PWM控制器,那输入输出电容GND和外置MOSFET电流采样RSNS的GND端就是功率GND;

    其余的UVLO下拉电阻RUV1、软启动Css电容、频率电阻RT、反馈下拉电阻RFB1、VCC电容CF的GND端和LM5022第6pin GND,这些信号GND是不是应该单独铺一块铜皮,然后再单点连接到输入输出及电流采样功率GND的大铜皮上呢?且我PWM的RC滤波GND端和电压跟随器的GND又该如何接?那针对我的应用PCB层数该设多少?(我目前预计用4层PCB),如何更好地PCB Layout才能高度稳定可靠?要注意哪些细节?请指导,谢谢!

  • 您好,

    关于您的新问题请重新发一个帖子,谢谢!

  • 好的,谢谢,刚已经重发。