你好,目前使用BQ2057TTS对两节串联的18650锂电池充电(单节的额定电压是3.7V)。充电输入电压Vin是9~100V可调的,所以先用芯片LM5017调整电压至10V,再用BQ2057对电池组充电。现在是可以实现充电,但充电到电池组电压约为7.6V时就停止充了,用示波器观察发现,电池电压瞬间升到9.4V,然后就停止充电了。拔插一下充电源,可以重新开始充电,但过几分钟又会停止,为什么会这样呢,远不到8.1V就停止充了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
15V是BQ2057输出的最大电压值,要根据cell实际的串数来提供充电电压。
10V可以给电池充电,电池在进入charging voltage 阶段的时候由于提供的电压拉太大,电池会进入过电压保护,就没有办法充电了。
数据手册开头就有说明:
Ideal for Single (4.1 V or 4.2 V) and Dual-Cell
(8.2 V or 8.4 V) Li-Ion or Li-Pol Packs