This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54560带轻负载问题



前辈们好,我是一个电源新手。最近在调试54560的时候遇到个也许是白痴般问题,希望前辈们不吝赐教。具体问题是这样的:

之前我有块带54560的板子是9~36V输入,5V/5A输出的(正常工作);现在我要将它改为40V输入,12V输出,负载估计在50ma~200ma之间。由于手里没有100uH的电感,所以就按照webwench推荐的4A的设计(电感要求为22uH)来改造旧板子。改造后发现电压输出正常,带我的另一块显控板子(功率需求12V 1A左右)也正常,但是带我的网络延长器模块(就是前面说的在50ma~200ma之间)发现网络延长器丢包频繁,但用别人的适配器(220V转12V 1A)工作正常。不知什么原因。也不知TI的Eco-mode模式的具体工作详情,是否在轻负载带载时有什么需要注意的??

另外还有个奇怪的现象:我用示波器探头或万用表表笔接触12V输出时,网络延长器丢包会明显好转(注:是明显好转哦),我也尝试过在12V输出端并联几PF到十几PF的小电容,但是没有任何效果,估计还是我的参数配置(补偿网络)或是Eco-mode模式带轻负载的问题,希望前辈们不吝赐教。拜谢!!