Part Number: TPS65994AD
Dual standard Type-C ports, both support Sink 20V/5A and Source 5V/3A;
the first Type-C port is primarily used as a Sink to connect a 20V adapter to power the motherboard, while the second Type-C port connects to an expansion HUB to output 5V/3A. At this time, testing the OCP of the second Type-C port shows only 1A, which cannot reach the rated specification of over 3A; if the first Type-C port is not used for power supply and another DCIN is used to provide the power path, then testing the OCP of the second Type-C port can reach above 3A.