Part Number: TPS4810Q1EVM
测试硬件平台:TPS4810Q1EVM
输入电源:12V@10A
负载:电子负载,恒电阻模式
测试描述1:在使用INP来使能测试和关断测试;初次上电后,MOS管默认导通;通过INP关闭MOS输出;
测试问题1:通过INP关断瞬间有正向电压过冲;
测试问题2:通过INP开启瞬间,电子负载无法工作,测试板故障报警;


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS4810Q1EVM
测试硬件平台:TPS4810Q1EVM
输入电源:12V@10A
负载:电子负载,恒电阻模式
测试描述1:在使用INP来使能测试和关断测试;初次上电后,MOS管默认导通;通过INP关闭MOS输出;
测试问题1:通过INP关断瞬间有正向电压过冲;
测试问题2:通过INP开启瞬间,电子负载无法工作,测试板故障报警;


我们也有尝试更换输入电压,更换为26V,还是会出现同样的问题;同时mos管在故障灯FLT亮起时有嗡嗡声;同时测试TP6和输入电压 波形,如下所示;TP6会有-6.8V左右的电压尖峰,这样就是所SRC网络此时电压约为56V左右。


测试环境描述
测试过程描述
故障描述