This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5050-1在 汽车诊断设备 测试过程中 失效

Other Parts Discussed in Thread: LM5050-1, LM5050-2

目前在设计一款带有平板的OBD检测仪,使用LM5050-1作为SS34的替代方案,测试过程中发现,电源电压高于20V 左右,会有BIAS电阻烧毁的情况, 失效的板子,bias电压只有1V左右,调整输入电压时,VS电压不变,当电压太高试,100欧姆电阻烧毁,IC功能也不正常。另外发现有LM5050-1.在OFF为5V电压时,没有关闭MOSFET的情况。

主要问题是,什么原因可能导致 LM5050-1 失效。

电源说明,分成两组,一组用过SS34 给诊断部分供电,  另外一组通过LM5050-1给平板供电兼充电功能。

另外两路电源 说明:一路为 DC 电源,充电用,诊断时不用;另外一路为汽车OBD电源 12V,诊断时用此电源供电。

lm5050-1.pdf