This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS4810Q1EVM: TPS4810Q1EVM: TPS4810Q1EVM在测试24V系统中频繁报故障

Part Number: TPS4810Q1EVM

测试硬件平台:TPS4810Q1EVM

 

我们也有尝试更换26V输入电压,还是会出现同样的问题;同时mos管在故障灯FLT亮起时有嗡嗡声;同时测试TP6和输入电压 波形,如下所示;TP6会有-6.8V左右的电压尖峰,这样就是所SRC网络此时电压约为56V左右。

测试环境描述

  • 输入电源26V,直流电源输入
  • 输出电源26V左右
  • 负载功率:电子负载恒功率模式100W左右

测试过程描述

  • 搭建测试环境,直流电源调整到26V,限流10A;关闭电源输出;电子负载调整至恒功率模式,100W,关闭负载;
  • EVM输入输出端接上直流电源和电子负载,另一台直流电源接INP/信号;同时示波器监测输入电源VIN和SRC网络TP6,其中黄色为VIN,蓝色为SRC;
  • 打开直流电源开关,输出26V;电子负载显示输出电压26V左右,然后打开电子负载开关,恒功率运行;
  • 然后通过INP/信号关闭mos,INP/上电给5V信号;然后再关闭INP/信号的上电,打开MOS;此时mos管无法打开,并伴随嗡嗡声,FLT亮红灯

故障描述

  1. 为什么在这种工况下,开关使能打开mos会无法输出,无法带负载
  2. mos管在这个期间,为什么会有嗡嗡声
  3. 为什么VS端会有高达56V的反向电压

 


之前的帖子

https://e2echina.ti.com/support/power-management/f/power-management-forum/1071024/tps4810q1evm-tps4810q1evm-12v