1、DOD更新时在relaxation mode,DOD0时在relaxation mode 等待30分钟后的测量值,更新中提到有可能没有DOD0的测量,是不是指relaxation mode没有30分钟,已经进入到下一个充放电mode,还是说有别的情况?
2、此时的DOD0就是上个relaxation mode的DOD通过充放电量的计算得到的,这个DOD值就是该relaxation mode没有等待30分钟更新的值,可以用来跟下一个relaxation mode的DOD计算更新Qmax
不知道这个理解对不对?
3、PassedCharge has to be more than 37% of DF:Design Capacity for an update to occur.For the first cycle (with DF:Update Status = 4), 90% of DF:Design Capacity is required.
这句话是要怎么理解,每次更新Qmax的时候还要判断一下充放电量么?