This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25120如何进入运输模式??

Other Parts Discussed in Thread: EV2400, BQ25120

 我们选购了TI的BQ25120EVM-731的板子,想进入运输模式(ship mode),我也按照测试步骤进行了,得到的电压不是100nA以内,而是415uA左右。

Ship Mode (Optional if I2C Control not Used)
1. Enable PS#1 and PS#2
2. Open the software GUI
3. Go to Field View of the GUI and then read all the registers. All the default register values should be
shown in the register map (as shown in Figure 3).
4. Measure on CM#2 → ICHRG = 9–11 mA
5. Install the jumper on J7 – connect CD to SYS
6. Disable PS#1
7. Measure on CM#2 → ICHRG = 5–7 µA
8. Check the box in front of “EN_SHIPMODE” in the software GUI
9. Measure on CM#2 → ICHRG < 100 nA
10. Disable PS#2

上面是说明文档里对进入运输模式的说明,第1~7步没有任何问题,电流表测试的结果也跟文档上说明一致。

第8步因为我们没有EV2400的板子,所以用不了GUI去调试。

但我们用自己的MCU编程给了它一个进入ship mode的指令。

具体是给0x00地址写了一个0x20的值给它,也把CD脚跟SYS短接了,并且拔掉了充电线。

结果电池处得到的电流是415uA左右,而不是上面说的小于100nA。


请问对上述问题有什么解决办法?在线等,谢谢!