LMR51635: LMR51635上电时输出保护异常问题

Part Number: LMR51635

我的使用的是LMR51635YFDDCR这个型号芯片,设计一个12V降5V的电路,电感和输出输入电容是按规格书推荐的,然后发现一个问题,正常上电,就是先插好输入座子,然后再开启电源12V,这时候是输出正常的5V,但是我先输出12V,再插入座子,输出就保护了,输出的波形是85ms周期性的波形,峰值大概1.2V,而且不会恢复,要重新上电才恢复。但是我的5V负载不大,再大才100mA,输入和输出的电容也是按手册推荐的。