This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2000: BMS芯片选型

Part Number: BQ2000

您好:

请协助选一款满足以下条件的BMS芯片:

充电限制电压:4.2V

放电终止电压:3.0V

推荐充电电流:75mA

最大充电电流:150mA

推荐放电电流:30mA

最大放电电流:150mA

上限充电温度:42℃

下限充电温度:32℃

标准充电:以05Cm恒流充电至42V,恒压充电至截止申流0.05Cmim