This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335供电方案



大家好,之前设计的F28335的供电模块使用的是TPS767d301,是一个+5V输入,+3.3v和+1.8V输出的电源芯片,我现在重新设计一遍,来模拟在汽车上面的应用,所以想用一个+12V转出+3.3V和+1.8v的芯片,而且满足F28335的上电逻辑,不知道大家有没有用过,请赐教。

其实也可以用,一个+12转出+5V,在使用TPS767d301,我尝试过这种方案,+12V 转+5V的芯片使用的是英飞凌的TLE42744,电压可以转出来,但是,程序在跑起来一会,大约30s,TLE42744就发热严重,请大家推荐一下电源方案,十分感谢!