This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ41Z50: BQ41Z50 learning失败问题

Part Number: BQ41Z50

Hi Ti team:

1.我使用CHEM ID:4191进行learning,充满和放空搁置时间分别为5小时,并已触发满充和满放标志位,进行多个循环的充放电,Max error还是为100,Qmax和Ra不更新,update status为04,这个是什么原因导致?个人分析如下:

1.

1. 确认已使用正确的 LFP ChemID

LFP ChemID选用库里面已有的ID,和电芯型号一样的

2.EDV0=2750mV;UVP=2650mV 

3.ResRelax Time=200s? 

4.learning 前已复位电量计

5.充电电流有要求吗?目前用的是0.5C ;放电电流目前用的是0.2C 

6.FC 标志位已触发 ,

7.静置需要多长时间?