目前在用BQ24773设计一个电池充电管理,附件是原理图,
有几个疑问:
1、21引脚ILIM是外接电路怎么设计,上拉电压多少,上下电阻多少?可以悬空吗?
2、是否在不接IIC的host控制端时接电池和适配器就可以进入充电模式(暂时不使用IIC,直接接适配器和电池)
3、7脚、8脚、9脚、13脚和14脚可以悬空吗?不悬空怎么接?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前在用BQ24773设计一个电池充电管理,附件是原理图,
有几个疑问:
1、21引脚ILIM是外接电路怎么设计,上拉电压多少,上下电阻多少?可以悬空吗?
2、是否在不接IIC的host控制端时接电池和适配器就可以进入充电模式(暂时不使用IIC,直接接适配器和电池)
3、7脚、8脚、9脚、13脚和14脚可以悬空吗?不悬空怎么接?
1. 21引脚可以通过REGN分压得到,总和最好大于100k. 是一个硬件限流,限流值是21脚的分压值除以20,再除以采样电阻。如果不用,建议不要悬空,上拉到REGN,。 硬件限流和软件限流0X3F 选取较低的一个, Input current limit is set by the lower value of ILIM pin and REG0x3F. <default at POR>
2.可以的,但是内部有一个寄存器,175s之后会挺,然后又重新以默认充电。
3. 7.8.9 脚可以悬空,13脚接GND, 14脚悬空。
Could you please give an example to explain? What does "采样电阻" mean? a resistor between the voltage divider and pin21?Xinming Gao 说:1. 21引脚可以通过REGN分压得到,总和最好大于100k. 是一个硬件限流,限流值是21脚的分压值除以20,再除以采样电阻。如果不用,建议不要悬空,上拉到REGN,。 硬件限流和软件限流0X3F 选取较低的一个, Input current limit is set by the lower value of ILIM pin and REG0x3F. <default at POR>
2.可以的,但是内部有一个寄存器,175s之后会挺,然后又重新以默认充电。
3. 7.8.9 脚可以悬空,13脚接GND, 14脚悬空。
Thank you.Star Xu1 说:
I am using a 100k resistor directly pull ILIM up to REGN, is it ok?
I am using a 4x battery pack, the ACOK=H, BATPRES=L could be get from default setup. While voltage difference between CMSRC and ACDRV is 5.03V, and the charging could not start by default setting, could you help to look into the issue?
Thank you.