This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在车上现有+12V的基础上,F28335电源模块设计

Other Parts Discussed in Thread: LMZ31704, TPS54340

大家好,上一次发帖可能没有把问题描述清楚,我再重新解释一下,希望各位大牛慷慨解囊,给我一些建议!

设计目的是给F28335供电(这款芯片需要+3.3V 和+1.8V来供电,这里选择的芯片是TPS767D301,已经测试过,这块芯片+5V供电后,会准确的转出+3.3V和1.8V,而且,dsp工作正常);

现在的条件是有一个车载电源+12V,怎样产生+3.3V,1.8V电压给F28335供电?,我现在的想法是+12V转出+5V,然后在转出+3.3V和+1.8V(这一步可以保证),就是+12V转+5V这一步比较头疼,因为板子上还有其他的一些+5V的负载,所以希望+12V转+5V的电流尽可能大一些,比如2A,当然这就涉及到效率和发热的问题,我不知道该怎么办啦,请各位支招!

之前有人建议给F28335供电最好是线性电源,我就选择了一款汽车级芯片,tle42744,它的最大输出电流是400mA,我在使用两块并起来的时候,F28335只要一工作,1分钟之后,TLE42744就会很烫,估计是输出电流的能力不够。请大家提供好的建议!在线等!