This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79616: ADC voltage acquisition failed

Part Number: BQ79616

HI,

I am debuggin the environment with BQ79600 and BQ79616。some issues have been encountered.  send the following command:

 {0x90, 0x01, 0x00, 0x03, 0x04 };   // active cell, 10s

{0x90, 0x01, 0x03, 0x0D, 0x06 };    // enable adc

{0x80, 0x01, 0x05, 0x68, 0x1F};      //  red cell voltage

--> response:

0x80 0x00 
0x80 0x00 
0x80 0x00 
0x80 0x00 
0x80 0x00 
0x80 0x00 

-------------------------
0xd4 0x54 
0x7a 0x13 

------------------------
0x44 0x5d 
0x44 0x27 
0x44 0x2b 
0x44 0x31 
0x43 0xfc 
0x44 0x16 
0x44 0x14 
0x44 0x07

the upper 6 cells are not enabled, and the next 2 cells' voltages are invalid. low 8 cell voltages are vaild.

 

  --> send the following command:

 {0x90, 0x01, 0x00, 0x03, 0x0A };   // active cell, 16s

{0x90, 0x01, 0x03, 0x0D, 0x06 };    // enable adc

{0x80, 0x01, 0x05, 0x68, 0x1F};      //  red cell voltage

--> response:

0x77 0x23 
0x7b 0x1d 
0x8c 0x89 
0x7b 0x10 
0x90 0xe9 
0xa3 0xda 
0xcd 0x3f 
0x79 0xfd 

------------------
0x44 0x58 
0x44 0x25 
0x44 0x29 
0x44 0x34 
0x43 0xfb 
0x44 0x14 
0x44 0x12 
0x43 0xfd 

low 8 cell voltages are valid, high 8 cell voltages are invalid.

the actual voltages on terminals VC0 to VC16 are all about 3.3V per cell。do i need to configure any other registers ?