This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5171: LM5171无法正常工作

Part Number: LM5171

LM5171设置为BUCK模式,VCC=9V  ,VDD=5V ,VREF=3.5V无波动。VSET和ISET 通过电阻分压,设置电压分别为2V,1.6V。频率100K,  IPK=1.7V,. EN=DIR=3.3V。芯片上电后,输出等于输入。并且COMP呈现幅值为2V,周期1ms的方波,SS/DEM使用22nF接地,测试SS/DEM脚电压,呈现三角波,最高值只到2.2V,周期800uS.。类似进入DEM模式,HO和LO都是无法正常输出PWM波。按照官网提供的DEMO原理图,设计的板子