Part Number: LM5149-Q1
Other Parts Discussed in Thread: LM5137-Q1
Hi Folks,
We need an LM5149-Q1 2-phase application. Could you provide us with a reference schematic for the 2-phase version?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We do not have LM5149-Q1 2-phase application schematic,
Take a look at the LM5137-Q1 two-phase controller - this is a much easier implementation with no need for external SYNC.
Hi,
You can check if "Figure 8-8. Schematic Configured for Single-Output Dual-Phase Operation" and "Figure 9-40. Application Circuit 4 With Two LM5149-Q1 Buck Controllers at 400 kHz" in the datasheet can meet your needs.
Hi Lydia,
Does the LM5137-Q1 dual output mean that each phase Iout is 20A?
Therefore, when designing the dual phase, should Iout = 40A?
My application conditions:
VIN: 24~70V (normal: 48V)
VOUT: 12V
IOUT: 40A (max), full load test estimated 32A
Thanks.
Hi,
Could you provide us with a reference schematic for the dual phase of the LM5137-Q1?
You can take a look at this document LM25137-Q1 Evaluation Module User's Guide (Rev. A) and LM5137F-Q1 12V, 20A Single-Output Evaluation Module
If you have any further questions about LM5137-Q1, please resend a post for other users to search. Thank you