我在使用BQ24133时发现:在适配器被拔出以后,ACDRV任然输出18V左右的电压,同事SW输出大概13V的电压?
充电电流正常(设定值为1A)。BATDRV驱动信号不正常,VREF电压正常3.3V
出现这种问题可能的原因是什么(一批次生产,有的是OK,有些不正常,希望找到原因,方便维修)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yi Mee
请查看一下BTST电容是否工作正常,方便的话也请贴出原理图,谢谢!
Hisen Zhang
ACDRV关掉的前提是VCC电压比BAT电压低,不知道你的VCC电压是不是通过两个二极管或在一起的,一个是输入电压,另一个是输出电池电压。