Other Parts Discussed in Thread: BQ27520-G4, BQ34Z100-G1
您好,我在寻找一款系统级应用的电量计芯片,目前看到BQ34Z100-G1和BQ27520-G4两种比较适合。
我的电池参数为锂离子电池,额定电压9~11.2V,额定电流10A,峰值电流30A,容量22AH,电池内部是3块电芯串联。
请问BQ27520-G4可以使用吗,使用时我准备通过电阻分压,把电池输出电压分为1/3,这样就相当于一块电池的电压了,这样是否可以?电流采样电阻应该按照10A设计还是30A设计呢?
另外看BQ27520-G4手册没有看到进行电池学习校准,与BQ34Z100-G1不太一样,那么BQ27520-G4是如何确保测量精度的呢?
BQ34Z100-G1适合多种电池使用,但应用比较复杂,尤其我在系统板上使用无法直接连接PC,不知道怎么对BQ34Z100-G1芯片进行学习,学习后怎么将数据下载到芯片。