This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM82864A: 替代TPSM82864A

Part Number: TPSM82864A

我们前期采用了TPSM82864A,芯片输出3.3V,但是测试发现,单节锂电池供电,负载电流2mA时,在电池电压从3.4V升至3.8V区间,82864芯片本身电流高达15mA,这个现象是不能接受的。

请帮助选择替代型号,要求:输出电压包括3.3V,输出电流≥3A,单节锂电池供电且轻载时,芯片本身电流尽量小,小于1mA是比较理想的情况

buck或buck-boost芯片都可以

请不要简单给我选型链接,因为有的参数在datasheet中并不显示,我们实测才发现问题

请基于对贵司产品的了解,推荐一些具体型号

非常感谢