Other Parts Discussed in Thread: UCC3895
您好!
我现在在用一快UCC3895的芯片做移相全桥,输入是DC400V,输出80V/50A,我想用这快芯片来做一些驱动,采样,在加上一快小的单片机来实现通迅和保护,可是我现在看这快芯片,有几个点不太明白,输出采样经光耦返回到EAP脚怎么会实现相移?那输出过压和欠压保护是哪里做的了?还有为什么RAMP为什么要经过个电阻到CS脚,我采用的是平均电流模式控制的,是否可以不接?我这个CS脚当输出过流保护是否可以?看资料上说把ADS和CS连接在一起,延迟时间为0,但是跟公式不符合啊?如果连在一起,那VDEL=0.5V,假如RDEL=10K,则根据公式可算出延迟时间为520NS?还有英文的资料上的曲线,当A=VADS/VCS=1的时候,不管VCS电压怎么变,死区时间为500NS?望请专家指导