This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: 放电末端和充电开始跳变问题

Part Number: BQ40Z50

BQ40Z50-R3芯片,做3串项目,(Term Voltage为9300mV,此为客户指定不可修改)客户主机为超薄笔记本电脑,以下参数可调整:Load Select为1,Fast Scale Load Select为1,Load Mode为0,RSOC_CONV为1,SMOOTH为1,RSOC_HOLD为0,RELAX_SMOOTH_OK为,1,Term Voltage Delta为300mV,Pack Resistance和System Resistance为0,SMOOTH为1,目前跑0.2C放电golden没问题,1C大电流放电,末端会3跳0,跳0原因是触发到9300mV,0%电压点,刚开始充电又会0%直接跳到3%。如何调整参数,解决跳变问题?