This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1使用疑问

Other Parts Discussed in Thread: BQ34Z100-G1

最近准备做一块电池管理板,板上用BQ34Z100-G1芯片做host-side或者说是系统端的电量计。电池充电时拔下,放电时通过电池管理板。电池共采购了同一型号的若干块,每次使用一块,可能会交替更换使用。

电池基本参数为: Lithium Polymer (LiPo) ;  容量 : 22Ah  ; 连续放电电流 : 10A ; 最大峰值电流: 30A ; 电池电压 : 8.25~12V

我的问题是:
1、通过EVM进行learning cycle后,Golden数据如何下载?是不是需要在我制作的板子上留出“SDA”和“SCL”端口,用于连接EV2300,再通过PC端软件下载?
2、通过PC端的EVSW软件可以更改和配置BQ34Z100-G1的data flash,按需要配置好以后,是否板上单片机不需要再配置BQ34Z100-G1芯片内的这些参数了?板子掉电后,这些数据应该是保存的吧?
3、IT算法需要电池接入的短时间内测量一次OCV,此时应该是无负载状态,但是因为我是一个系统端应用,电路板上还有其他电路,比如DSP等,此时电流比较小,估计大约20mA左右,会影响IT算法的精度吗?
4、我的用法会经常拔掉电池,使用时再接上,甚至更换另一块相同型号的电池,这样是否会影响电池容量的估算精度。我理解相同型号电池的放电特性应该几乎一致,但是Qmax参数与寿命等有关,可能不同电池会不一样,这样更换了电池,会导致估算出现偏差,我的理解是否正确?