对于LM5069_2热插拔芯片:
UVLO脚的两个电压VUVH和VUVL中,VUVL比较好理解。但VUVH应该怎么理解?
对于DS中给出的连接方式,R1和R2分压接入UVLO,串接一个5K的电阻是否可行?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请参考LM5069 datasheet的16页Figure.12,UVLO脚内部有一个21uA的hysteresis current,此电流使UVLO有VUVH和VUVL之分
OVLO也一样
你好,TI员工:
我现在这个项目十分紧急,用你们的LM5069做的方案:10V到36V输入,TIMER电容用的是105,PWR电阻用的是68K的电阻,GATE驱动电阻10R,mos管用的是FDD2582,150V耐压的,21A,现在有个现象就是:30V多一些的启动电压,会把mos管烧毁,GDS全导通,低压启动时,30-36V正常工作,当达到36V保护点时,芯片GATE输出低电平,然后将输入电压调至35。5V多一些,芯片重新启动,这个时候mos管基本都会烧毁,GS之前并了一个10V的稳压管,后来又换成4.7V的稳压管,还是会烧毁mos,请您帮忙分析一下,十分紧急!!我的QQ:258481469,电话:13003994971