This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TL494 PWM最大占空比问题

Other Parts Discussed in Thread: TL494, LM3481, TL5001

选用TL494设计BOOST电路。需要将2V-5V的s输入。输出要求达到13V,估算90%可以满足要求,,于是将TL494输出并联,使其能满足要求、

PWM频率为200KHZ,此时测的的最大占空比为81%,100KHZ是最大占空比为84%。

回头看了下手册发现,说明的最大45%(单个),实在频率为20KHZ时测的。。。

之后百度,有人说可以最大调到94%。

我的死区输入电压是通过2K电阻接地的。供电12V,RT=5.1K,CT=1NF。

请问有什么解决措施么、