This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51430EVM: LMR51430EVM抽電流1.5A 壞掉(30.8V->5V)

Part Number: LMR51430EVM
Other Parts Discussed in Thread: LMR51430,

我使用LMR51430EVM 都沒有更換EVM元件,輸入30.8V,輸出5V,單我掛上負載開始抽電流1.5A,輸出電壓=0V, 但是將負載移除的時候,輸出依然可以量到5V,後來我將LMR51430更換之後又可以抽電流1.5A,但是output電壓掉到剩下4.5V, 我之前是輸出抽電流1.5A,但是壞掉3顆了....壞掉現象都很一致 當抽電流(掛附載)

時候輸出都是0V,電源供應器(輸入)也沒有看到大電流現象. 我另外一片是使用 5.5 to 3.3V  輸出電流使用1A 就很穩定輸出....