BQ25750: BQ25750在没有接电池的情况下检测充电

Part Number: BQ25750

我把电池充电电压设置为20V,然后用直流稳压电源13V进行充电,但是电池接口的电压只有16V左右跳变,然后直流稳压电源的界面显示输入电压13V也是在跳变的。然后我把直流稳压电源设置为15V,界面就没有跳变了,但电池接口端的电压变成了15V,还是没达到我想要的20V。我电池电压值是通过分压电阻设置的,电池充电限流2A,输入限流40A也是通过电路设置的。软件的寄存器我只禁止了看门狗和TS。我想知道这种现象正常吗,在没接电池的情况下。