This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: BQ28Z610量产烧芯片

Part Number: BQ28Z610
Other Parts Discussed in Thread: EV2400, BQSTUDIO

你好,

我在进行BQ28Z610量产固件烧录时,出现了两种情况。

一种是一开始可以通讯,固件烧录进行到一半显示烧录失败,并且无法进行通讯,概率为5%;

另一种是可以正常进行烧录,再次连接上位机进行数据检查时,无法进行通讯,概率为20%。

经过排查确定都是芯片损坏,我想问一下造成这一结果的原因是什么。

谢谢!