This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62903: EN和输入输出电容的问题

Part Number: TPS62903

你好,ti专家团队:

准备把62903用于12V转5V和1.8V这两路电压转换,有2个问题:

  1. 需要用EN和电阻分压实现对VIN的UVLO功能,如VIN需要>=10.5V,EN才有效。DATASHEET里查到EN-PIN的VIH和VIL是2组值,接近但不重合,这样可以直接设计出有回差的VIN UVLO功能吗?也就是VIN>=10.5v确定一组分压电阻,然后用VIL计算出VIN<=某个电压时DC/DC关闭。
  2. 输入10uf和输出22uf电容,要求是静电容还是DC BIAS后的有效电容?查了表8-1里的CIN和COUT,有效电容都是低不少的。
  3. 表7-3,是说只有VIN>1.8V后,PG才能确定的状态吗?